Other Parts Discussed in Thread: TEST
I would like to ask about the LED output state when the LED output is stopped.
①Set LED output duty to 0% when EN = Hi
② LED output is forcibly stopped when EN = Low
Is there any difference in the LED output status between these two methods?
(For example, is the phenomenon that the LED output does not turn off and lights up for a moment using the method of ①?)
Best Regards,
Y.Ottey