BQ25887 has a 16-bit ADC.However, when I tested the BQ25887EVM board, the voltage error was 18mV.
As shown below.
BQ25887 detection
Is there any way to calibrate this voltage?
Thank you very much!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ25887 has a 16-bit ADC.However, when I tested the BQ25887EVM board, the voltage error was 18mV.
As shown below.
BQ25887 detection
Is there any way to calibrate this voltage?
Thank you very much!
Skate,
The integrated ADC measures this voltage directly at the pin. I see from your photo your are measuring at the screw terminals of the EVM. This is not a good practice as there is a small voltage drop from the trace resistance between the IC and the terminal.
Please retake the voltage measurement as close the the IC as possible, and let me know if you are still seeing the inaccuracy.
Thanks,
Ricardo