Other Parts Discussed in Thread: TPS610985, TPS61098, TPS610987
Hello there,
We have a power source which gives 1.5V at approx 20-30uA current. We want to regulate this supply to 1.8V so we are considering using TPS61098X device in low power mode.
We are doing some testing with TPS610985 EVM, but we are not able to get 3.0V at VMAIN node in Low Power mode, in no load condition. The VMAIN node goes up-to 1.3-1.4 V and starts dropping the voltage again. The input voltage is observed to be 0.42 V and VMAIN is settled at 0.4V in this case.
What is the start-up power/current requirement for the chipset?
We will never use the device in active mode, in that case is it better to consider TPS61098 and TPS610987 for our application which has VMAIN=2.2V in Low Power Mode?
What can be the maximum value of series resistor for VIN pin and maximum value of pull-down resistor for MODE pin?
Thanks,
Nimesh