Hello,
We would like to use the TPS65132S in an application where we want +5.2V and -5.2V… however the default values are actually +5.4 and -5.4V.
The datasheet indicates there is an EEPROM internal to the TPS that can be written to for different default start up values.
- So we would only need to program the output voltage 1 time, on first startup of the device, to program +/-5.2V?
- After this programming then we will always have our desired +5.2/-5.2 Vouts by default (like during production)?
Thank you, Keith