Other Parts Discussed in Thread: LP38842, TPS74401, TPS7A10
Hello team,
I am looking for Low drop/ low Vout Voltage regulator with the following requirements:
Vin=1V; Vout =0.815V; Iout=1.35A
Vref about 0.7V and below and Vdrop (max) < 150mV
The LP38842 is the best LDO that I found, But the drop voltage may be more (1V-0.815V=185mV) up to 315mV.
Could you please suggest another device which meets the requirements above.
Thanks in advance
Best regards,
Shai