Other Parts Discussed in Thread: UCC256404
Hi Sir
If new project ,could we use UCC25640x to instead UCC256301 ?
But I don't see UCC256401 on TI website ? Could you help to double confirm ,which P/N could instead UCC256301
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kai,
UCC256404 should work well in place of UCC256301. UCC256404 will have a different BLK start threshold than UCC256301 but contains many of the same features as UCC256301 such as HV startup, X cap discharge, etc.
Best Regards,
Ben Lough
Hi Kai,
Here is comparison table:
UCC256301 | UCC256404 | |
Burst Mode Algorithm | •15 pulses in each burst packets | •40 pulses in each burst packets |
•Burst soft-on and soft off | ||
•User option to disable burst mode | ||
•User adjustable burst mode hysteresis | ||
HV Startup | Yes | Yes |
X-Cap Discharge | Yes | Yes |
Minimal Detectable Slew Rate | 1 V/ns | 0.1 V/ns |
ZCS Protection | Yes | Yes |
BLK Start | 3.05 V | 1 V |
BLK Stop | 0.87 V | 0.9 V |
RVCC | 12 V | 13V |
OCP 1/2/3 | 4V/0.84V/0.64V | 4V/0.6V/0.43V |
Best Regards,
Ben Lough