This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74202-Q1: Can OUT pin be negative in shutdown ?

Part Number: LM74202-Q1
Other Parts Discussed in Thread: LM76202-Q1,

Hello,

When the LM74202 or LM76202 is in shutdown (/SHDN low) the power FETs are off.

Can the voltage on the OUT pin be negative (below GND) in this condition?

I would like to use the part as a current limited ideal diode and there is the possibility that the load will be a negative voltage (e.g. reverse battery) so I would shut down the part in that case.

Thanks for any help, Ken