Part Number: BQ24165
Other Parts Discussed in Thread: BQ25606
Hi,
I use the BQ 24165 to charge a single cell 46Ah Li-ion battery, Vcharge=4.2V. R=330ohnm (1.5A) between ISET and GND. As the safety timer is limited about 6h(typical 360 min), but the charge time for full charge is more than 6h. So the charge cycle stoped after 6h for my battery to charge from 3.7V to 3.996V and is not full charged. Another logic should be added to enable CE1 and CE2 and start another charge cycle while I am not willing to.
1. The time for safety timer can be modified or not?
2. Does there any pin can detect the wrong state for output ? CHG is just the indicator for charge cycle
3. Does there have a longer safety timer device which is pin-to-pin compatible to BQ24165?
Thanks a lot.