Other Parts Discussed in Thread: BQ25150, EV2400, BQSTUDIO
Hi,
1. Currently I am using BQ25150 TI EVM, but don't have battery.
2. Connected /CE pin to ground.
I want to do charging ON/OFF by I2C ICCTRL2(-> bit 0th) register.
When i write 0 on ICCTRL2 (-> bit 0th) then write operation is successful, but CHRG_CV_STAT bit from STAT0 register not set(active).
& same for setting Current limit to 100 mA, IINLIM_ACTIVE_STAT bit from STAT0 register not set (active).
why ??
I want to cross check of my operation by reading status register.
Is there any battery dependency ??, or other way to do that ??
Thanks & Regards
Akshay P