Hi TI experts,
We have the following problems
We test the semi-finished product OK, ultrasonic sealing after the occurrence of these conditions
1. The meter will not refresh (it will not scroll in the column of Value)
2. When the battery is connected, the rolling can be seen. However, when 500mA is used for discharge, the average current parameter will not be updated, and it is still 0.
3. The battery can communicate normally when connected, but the average current does not return to 0
Version used: 1.2.0