Other Parts Discussed in Thread: TPS2373
Dear Team,
The customer is looking for .at+.bt current sharing.
Do we have TPS23754(at)+TPS2373(bt) current sharing circuit for customer reference?
BR
Kevin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kevin,
Is customer looking for 50/50 current sharing? If AT+BT then the max power with 50/50 current sharing is 51W before the AT switch exceeds its max power rating.
If so, I recommend looking at PMP5236 as a reference which uses current sharing controllers. This is an AT+AT design but customer can modify it to AT+BT if they change the other converter with BT PD + PWM controller with same output voltage.
Or is customer looking for power sharing? Where the max power output will be AT+BT or 25W+70W=95W?