This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2557: ILIM pin voltage

Part Number: TPS2557

In the datasheet I see "The TPS255x uses an internal regulation loop to provide a regulated voltage on the ILIM pin. " .

can you let me know what is the range of the voltage on ILIM pin?

--Nikhil

  • Hi Nikhil,

    Datasheet only indicates the ABS value (-0.3V 7V).

    I think you can have a test with the recommended resistor range (20kohm  187kohm) @(500mA  5A) load.

    For TI's policy, I will first click resolved button.

    If you have any other concern, contact me any time.

    If you think resolved, please help click 'Issue is solved button'.

    Thanks

    Ziv