Other Parts Discussed in Thread: BQ25713, BQ24753
Hello!
Im building a system with bq24753A for battery charge and power path application. My input current Iadapt varies from 0.5A to 1A and my system current Isystem also varies in time. As I set Adapter Iadapt and Battery Ibat current with resistors (SRSET and ACSET), sometimes I have a situation, when Ibat + Isystem > Iadapt. In this case, charger is switching to the battery input. For that I implemented the DAC setup for current limits. Anyway, sometimes I have a situation, that Isystem > Iadapt and in this case battery provides the power for the system.
I am wondering, is it possible to build a design in the way, that in case Isystem > Iadapt, all the power from adapter still goes to the system and the rest is taken from the battery? Would it be possible with BQ25713?
Thank you and best regards,
Daria