This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS74401-EP: DROPOUT VOLTAGE vs IOUT Relationship

Part Number: TPS74401-EP

Hello,

I am planning to use TPS74401MRGWREP.

The design configuration as follows,

1. Vin = Vbias = 3.3V

2. Vout = 2.5V (Vin-Vout = 0.8V)

3. Iout = 2.3A

But in Typical characteristic Dropout voltage vs Iout relationship, Dropout is increasing as output current increases.

And my Question is,

1. will this regulation required high dropout at full load condition

2. Will it work for the above configuration, Because Vin-Vout=0.8V

Thanks,

Ramesh M