This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62085: Fail to build up voltage when setting load to CC at 2A

Part Number: TPS62085


Hi Team,

     My customer uses Chroma 6312 series E-load to test the TPS62085 EVM.

     The configuration is listed below.

     Vin=3V

     Vout=1.2V

     When setting E-load to CC mode at 2A, TPS62085 failed to build up the output voltage during booting on.

     But if adding E-load after booting on, the output voltage is normal.

     It's kind of you to look into this problem for us.

Thanks

Sincerely, 

Edward