This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27426: The difference of QMAX is huge on the units that are using BQ27426 for 12000mAh battery

Part Number: BQ27426

Hi,

Why is the QMAX highly different on two units

This is for unit #1: QMAX is 6924mAh

                                                                      SOC  Volt   AverageCurrent     RemainingCapacityFilter   RemainingCapacityUnfilter    FCCFilter  FCCUnfilter QMAX

<6>[ 658.459902] bq27x00-battery 1-0055: 100   4170    -815                     9993                                   4737                                      10292          4881             6924 

This is unit #2: QMAX is 12000mAh

                                                                     SOC  Volt   AverageCurrent     RemainingCapacityFilter   RemainingCapacityUnfilter    FCCFilter  FCCUnfilter QMAX

<6>[ 44.039884] bq27x00-battery 1-0055:   100   4101  -753                        9807                                 8254                                       8646            8487          12000