This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61093: TPS61093 Vout=15V at 200mA can be acheivable?

Part Number: TPS61093

Hi,

Can i able to achieve Vout=+12V with Iout= 150mA atleast,  Actually my Load requires 100mA , so for a safer side I was thinking of to have a Source current atleast 30% to 50% more than what the load consumes? Can this be achievable with  TPS61093, what could be the effeciency if I operate at 150mA of the system.