This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24715: Minimum system voltage

Part Number: BQ24715

Hi,

I have a li-ion 3s2p configuration.with minimum system voltage as 8.7 V.

the minimum system voltage in the datasheet Page 6 says that the minimum system voltage for 3s configuration is 9.216V. Is it fixed value? or can it be changed and set to the required system voltage? if so, how can i set the min system voltage to 8.7V?

Thank you

Regards 

B.Harini Krishna