Hello. I have a question.
The LP8758-E0 looks good for my FPGA power supply.
I need a total of four power rails : 1.2V, 1.8V, 2.5V, 3.3V.
But the LP8758-E0 is set to 1V, 1.2V, 1.8V, 2.5V.
The LP8758-E0 uses OTP, so the default power is determined unless I modify it.
I want to get the power I want when I turn it on.
But our company is so small that we don't need large quantity.
I haven't asked you, but I think it would be necessary to meet the minimum quantity to change OTP.
So I'm trying to change the voltage by hardware without any modification, so can I use the power feedback signal to divide the voltage?
According to the datasheet ... VOUT0: 1000mV.
If I design this as a circuit it looks like this ...
If I want to output 3.3V to VOUT0, can I change it as follows?
Then please check.
Thanks.
KYU.