This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61222: The output of the rectifier circuit is 2.22V, but the current is only 2-3mA. The cascade boost chip cannot work normally. Is it because of the current?

Part Number: TPS61222
Other Parts Discussed in Thread: BQ24002

I have the following questions
1. The manual of TPS61222 states that the ISW switch current is limited to 200mA. Does it mean that 200mA is required to make the chip work properly? The results of my tests seem to require that the input current be greater than 200mA
2. Does the quiescent current in the data sheet refer to the current value during normal operation after turning on the MOS transistor?
3. What does the output ILKG_VOUT leakage current 1uA mean?
4. The output of the rectifier circuit is 2.22V, but the current is only 2-3mA. The cascade boost chip cannot work normally. Is it because of the current?
5. Can you recommend some boost chips that require a small input current, thank you

  • Dear User:

    1. The manual of TPS61222 states that the ISW switch current is limited to 200mA. Does it mean that 200mA is required to make the chip work properly? The results of my tests seem to require that the input current be greater than 200mA.

    No, it's the peak-peak current of the inductance. The average current is smaller than half if in DCM with so light load. But during the startup, the circuit need to charge the output capacitance. It needs enough current to charge it. It could be hundreds mA depends on the components.


    2. Does the quiescent current in the data sheet refer to the current value during normal operation after turning on the MOS transistor?

    The quiescent current is testes without switching. Here is an application note clarify it clearly. http://www.ti.com/lit/an/slyt412/slyt412.pdf?keyMatch=WHAT%20THE%20IQ&tisearch=Search-EN-technicaldocument


    3. What does the output ILKG_VOUT leakage current 1uA mean?

    The spec is tested with "VEN = 0 V, VIN = 1.2 V, VOUT = 3.3 V". Measure the current flow into the VOUT pin. 


    4. The output of the rectifier circuit is 2.22V, but the current is only 2-3mA. The cascade boost chip cannot work normally. Is it because of the current?

    What's your power supply now? Could you test with enough input current capability supply? If the issue is still exist, please catch the waveform of the Vin, Vout, SW, and Icoil.
    5. Can you recommend some boost chips that require a small input current, thank you.

    May you share more details information about your application and requirements? So that I can give better suggestion. 

  • thanks for your reply.

    Because the voltage received through electromagnetic induction is relatively small, a rectifier circuit is used.
    After rectification, the output voltage is between 1-2V and the current is only 2-3mA. I want to use a charging chip with a power voltage of 5V to charge the lithium battery, so I want to add a boost module in the middle.
    Because the output current of the rectifier module is relatively small, the TPS61222 cannot work normally
    So I hope you recommend a boost chip with an input current of 2-3mA, which can increase the voltage from 1-2V to 5V

    best wishes

  • Dear user:

    You could add a supercap to smooth the current ripple. It's hard to find a part with peak current smaller than 10mA during the startup. It will be much easier if there is another routing to supply the startup current. 

    What's your application used for?

  • Dear User:

    As long time not hear you, I assume you have solved the issue. I'll close this post.

    If not, just reply below. Thank you~

  • I'm so sorry

    I have a new question.

    ccording to the parameters of the data sheet, the corresponding 0603 package capacitor and coilcraft power inductor are selected, and the output can reach 5V, but once the load is added, the voltage will become lower. What is the reason for this?

  • Dear User:

    May you share more detail information about the issue? What's the load condition and the Vin capability?

    May you catch the waveform of the Vin, Vout, and SW?

  • Dear User:

    As long time not hear you, I assume you have solved the issue. I'll close this post.

    If not, just reply below. Thank you~

  • hi
    I have a question
    BQ24002 data sheet indicates that VCC current is 1mA
    60mA when output current is precharged
    But when I use the actual circuit, I find that the output current is related to the input current. When the output current is 60mA, the input current must also be maintained at 60mA. What is the reason for this?
    Can you recommend some current charging chips

    Thank you
    best wishes

  • Dear User:

    I'm sorry that the BQ family is support by other team, and I'm not familiar with that. 

    You need to make a new post with that part and they will help you. Thanks for your kind understanding.