This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3780: Is this device suitable for debounce application?

Part Number: TPS3780


Hi,

my customer was using ADM1184 for debounce application.

Since TPS3780 is the most similar devices in spec(regardless of the channel number). 

But I can't see any parameter related to glitch at the SENSE pin.

There is only parameter of SENSE (rising) to OUT propagation delay, and SENSE (falling) to OUT propagation delay.

I wonder if SENSE pin voltage dips below Vit- for a very short time less than "SENSE (falling) to OUT propagation delay" and then rises above Vit+, will OUT ignore such dip and keep constant?