Dear Sir,
Please help to fill IC type in "F" Field of sheet 1 for attached file. The rule at sheet 2. Thanks~
Best Regards,品名--TI.XLSXSam Shyu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
Please help to fill IC type in "F" Field of sheet 1 for attached file. The rule at sheet 2. Thanks~
Best Regards,品名--TI.XLSXSam Shyu
Hi Sam,
The UCC28950 is a phase shifted full bridge controller which is usually used at power levels of 500W to several kilo watts. It achieves zero voltage switching at higher loads and is usually run from a 400V DC Bus from a PFC stage.
Regards
Peter