This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61230: The TPS61230 provides only 2 amps of current? "5A Switch Amp" misled me?

Part Number: TPS61230
Other Parts Discussed in Thread: TPS61088, TPS55340, TPS61089

Hi,

My input source is 18650 Li-Ion Battery. It has 10Amps output current capability (also has 3.5-4.2V Voltage).

I need 5V with 5A capability. I am trying to use TPS61230 with a Typical Application schematic.

It has 5A switch, but it does not supplying 5A, just supplying 2A. When amps rising from 2A, it shut down himself.

What is your suggestion? Should I change the schematic? Or another part number?

thanks.