This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2596: Analog Load Current Monitor equation

Part Number: TPS2596


Section 8.3.4 of the TPS2596 datasheet explains how to determine the load current based on the voltage across Rilm.

I'm trying to deduce the voltage range seen across this resistor, but do not seem to get to realistic results.

For example, suppose: Rilm = 511 Ohm, which limits Iout to around 1.78 A according to equation (5).

If I would rework equation (6) to Vilm = Iout * Gimon * Rilm, then with an average value for Gimon of 656 uA/A and at maximum current, I would get a Vilm of a little less than 597000 V, which is obviously incorrect.

I've checked the values several times throughout the datasheet, but cannot seem to find the source of my error. Can anybody shed some light on this?