Hi,
The applacation is as below.
1. PIM_3V3 connect to IN2, 3V3_STBY connect to IN2, D2 to GND, D1 to 3V3_STBY_PG. If 3V3_STBY_PG is high, the Vo=P3V3_STBY, otherwise Vo=PIM_3V3, right?
2. From datasheet, I see their are some daley during the tansisation time, to prevent IN1 IN2 conduct, I suppose their should be a small time slot the two MOS is swtiched off, so during this time, only the capacitor inside is providing the power? Will these be risks if the load is requiring big current? Do you have some suggestion?
Thank you.
Penn