This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Should we scale and calibrate the current before or after the learning cycle?

Part Number: BQ34Z100-G1

If the actual current of my equipment is greater than 32 A and needs to be divide by 5 times.

When calibrating the current, I set the loading current as 5A, and type in the value of -1000 in Gauge.

Should the above calibration happens before or after the learning cycle?

Can I calibrate the current in 1:1 ratio before the learning cycle, and divide it by 5 times after the learning cycle ?

Or should I divide it by 5 times before the learning cycle?

Thank you.