Other Parts Discussed in Thread: LM3481
Hi team,
My customer find a failure on LM3481 board, and the resistance between VCC and GND is 1.9 ohm, and the 10 ohm resistor(R23) of RC filter in front of the Vin is burned down. Now they try to reproduce the failure, and they connect the VCC to GND. The 10 ohm resistor is burned down, and the resistor between the Vin to VCC is decreased from 3.4 Mohm to 5.87 kohm.
As I know, the VCC is derived from the internal LDO, does this LDO has a internal current limit, as the VCC is shorted to GND? If so, the resistor(R23) of the RC filter should not be burned down when VCC is shorted to GND, then why the R23 is burned down?
The second question is, If I connect 10V to VCC to simulate the EOS of VCC when the board is normally working with 0.9A load, will this cause the 10 ohm resistor burned down?
Similarly, if I connect a negative voltage beyond the absolute maximum rating, will this cause the resistance between VCC and GND decrease to a very low resistance?
Your answer will help me a lot, thank you!
Gary