HI Ricardo!
If I want to test whether USB CDP can be used,How do I change my EVM connection?
The portable device outputs a nominal 0.6-V output on the D– line and reads the voltage input on the D+ line. The portable device concludes the equipment is connected to a CDP if the data line being read remains less than the nominal data detect voltage of 0.3 V. The portable device concludes it is connected to a DCP if the data line being read is greater than the nominal data detect voltage of 0.3 V.
How can I get this 0.6V voltage?I try to put D- in PULL-UP, D + in PGND,but it doesn't work .It still works in SDP mode.
Another question,When calculating the output capacitor, what is the ripple voltage △VSYS of the power supply? The calculation formula given in the data sheet contains CSYS. Isn't this the value I asked for.At the same time, I also want to know the calculation method of PMID capacitor(C9)and SW capacitor(C14).
Best regards from China,
Zhetao Xie