Part Number: BQ24002
Other Parts Discussed in Thread: BQ24040, BQ24072, BQ21040, BQ24232, BQ24090, BQ24083
hi
I have a question
BQ24002 data sheet indicates that VCC current is 1mA
60mA when output current is precharged
But when I use the actual circuit, I find that the output current is related to the input current. When the output current is 60mA, the input current must also be maintained at 60mA. What is the reason for this?
Can you recommend some current charging chips
Thank you
best wishes