Hello, I have a basic question concerning junction temperature on my fet and also concerning duty cycle.
I plan to use CSD18542 on the power block for a 3Phase motor. The motor draws current in the order of 1.4A for about 50ms. The Period I (hopefully correctly) calculated from the image shown below at ~ 80ms. Which makes the duty cycle 0.62.
The image was obtained by using a clamp current probe on phase A. Can you let me know if this is how u would have calculated the duty cycle.... that is the time any one of the 6 fets are conducting?
also, can I calculate Tj like this: Tj = Tc + Id x Vds x D. Where D is the duty cycle.