Hello,
The TPS63061 clearly specifies "Due to the 4-switch topology, the load is always disconnected from the input during shutdown of the
converter".
On our design the issue is that the input power supply could goes down because it does not have enough power for the load.
Does the TPS63061 disconnect the load when Vin is lower that 2.5V (it is a sort of shutdown)?
If the TPS63061 shutdown because Vin is too low, how long will it take to restart?
Is there a risk of rapid cycling?