Other Parts Discussed in Thread: UCC28881,
Hi,
I am using these two chips in an isolated Flyback converter (Vin = 300V, Vo=700V) and with the same transformer (Lpri = 5mH; n=1:2) I get different results.
When I use UCC28881 everything is perfect and I can charge the output capacitor at 700V fast enough as needed by the application.
However, when I change the IC to UCC28880 (which has a lower current limit) the primary current is somehow disabled and I see only an spike for about 200ns (it is not the lower current limit of this chip or the transformer saturation).
Now, when I change the input voltage to 200V, I clearly see a ramp-shaped input current but with higher oscillation as compared with UCC28881.The oscillation frequency is around 500KHz.
Cin = 100nF
L_primary = 5mH
Can one of you experts please help me to find out the reason for these oscillations and resolve the issue?
V_IN = 300V, CH4: Primary current of Flyback transformer, CH2: Drain-source voltage
V_IN = 200V, CH4: Primary current of Flyback transformer, CH2: Drain-source voltage
Please note the oscillation (around 500KHz) at the very start of the primary current ramp which is not damping fast either.