Tool/software: WEBENCH® Design Tools
Hello,
I'am using the TPS5401DGQR DC/DC converter with the following working ranges:
VIN_min = 4,5V
VIN_max = 30V
The WEBENCH® tool suggests to use the following voltage divider for the ENABLE pin:
RenT = 105kohm
RenB = 46.4Kohm
By doing this the maximum voltage drop on ENABLE pin would be arround 9V when Vin is 30V, but in the datasheet it is written that the maximum voltage on ENABLE pin should be 5V
How is it possible should I trust in the simulator?