Other Parts Discussed in Thread: TPSM84424
Hi TI team,
I'm using the following regulators of TPSM family in our upcoming board.
TPSM family:
TPSM84A22: 1.9V@10A
TPSM84A22: 1.5V@10A
TPSM84424: 1.8V@4A
TPSM84424: 3.3V@4A
TPSM84424: 1V@4A
TPSM84424: 1.2V@4A
TPSM84424: 2.5V@4A
Kindly verify the attached schematics for the above circuits.
Thanks and Regards,
Binayak