Part Number: TPS61071
Other Parts Discussed in Thread: TPS61073, TPS61070
Hi TI
I hope that you can help me understand a phenomenon, that I have not seen before.
It seams that the load response/transient of the TPS61071 differs randomly to the same switching load
setup:
V_in=3V
V_out=5V
load:
80mA
f=1Hz
D=50%
In the image below: Ch1=V_in, Ch3=I_out and Ch4=V_out
Adding output capacity solves the problem, but I would very much like to know the cause of this behavior??
I would appreciate any information you can provide on this subject.