Other Parts Discussed in Thread: TLV3691, TPS61023
Hello sir,
We are plan to use TLV3691 comparator and TPS61090 boost regulator in one our project.
Super Capacitor is the source of power which is given to the TPS61090 Regulator as a input .The range of Super capacitor charge upto - 4.2 volts.
Our requirement is to enable the TPS61090 Regulator if Super capacitor voltage reaches to 4 Volts and disable the regulator the Super capacitor voltage below 2V.
Evey time TPS61090 Regulator should be enable once Super capacitor voltage reach to 4 Volts.
Give me the better solution to implement above concept with 2V of hystereris.
Regards
Lakshmanan V