This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25924: Question of Accuracy Specification of of Current Limit Specification TPS25924

Part Number: TPS25924
Other Parts Discussed in Thread: TPS2595, TPS2596

Hi Sirs,

According to the TPS25924 datasheet page 10, over current limit accuracy is 30% with configuration at 1.0A. Does it mean that the over current protection threshold will be between 0.7A and 1.3A with 1.0A configuration? If so, the specification may not be acceptable for customers. Would you please advise tips to improve the accuracy?



Thank you and Best regards,

Wayne Chen
12/20/2019