I used LM5008A designed a circuit ,used a application of TI MD015A's example to convert 24v to 12v,but my inductor is hot soon ,i don't know why ,how can i correct this design?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I used LM5008A designed a circuit ,used a application of TI MD015A's example to convert 24v to 12v,but my inductor is hot soon ,i don't know why ,how can i correct this design?
Hello,
What is the saturation current of your inductor? You must make sure the saturation current is well below the peak ripple current.
Please double check that or share the part number with me,
-Orlando
What output current are you running at?
For both those inductors the rated current is similar (0.65A) and with that current the temperature rise ΔT will be 40C.
Does it get hot at no-load?
Now i have solved that bug,but now LM5008A does not have a output?why?I have test the input ,it provise 24v,but no current input,only pin8 can test 24v,but other pins can test nothing,why?
it get hot at no-load,ihave solved the bug ,because it has a short circuit,but when i solved that problem,with a new PCB but new problem just LM5008a doed not have a output have occured?why it does not have a output?which aspect can i tackle this situation?
Are you using the same schematic?
If you have no VCC voltage, then potentially there is an issue with your chip grounding, or maybe a VCC short.
Please be sure your new PCB does not short the VCC pin to any other pin and the GND is correct.
Once VCC is fixed the chip should work correctly.
-Orlando