This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54917: Bode Test Review

Part Number: TPS54917

Hi Expert,

I have a question that when we measure bode plot and see gain across zero not only one time, shall we measure 1st or 2nd point for phase margin?

For example we did test on TPS54917 with Cff=680pF and see 1st Fc=28K and 2nd Fc=45K(File: Vim-4YE-220P). Which one is what we need?

Sometimeswe see phase across zero not only one time for example file: Type 2. Which one is what we need to measure for gain margin?

Could you please have review if the result is good? Thank you.

tps54917.7z