Other Parts Discussed in Thread: PMP20660
Hi team
We have constructed a battery charger circuit for CC/CV using LM34936-Q1.
When the input and output voltage are similar, I noticed a strange part of the current waveform.
- Normal condition
- Input voltage : 8~16V
- Output voltage : 13.5V
- Output current : 10A
- Schematic : http://www.ti.com/tool/PMP20660?keyMatch=PMP20660&tisearch=Search-EN-everything&usecase=part-number#0
- I designed the circuit by referring to the PMP20660 circuit on the TI site.
As shown above, three types of waveforms are output.
Question
- Please explain the above waveform.
- Can you improve these waveforms?
Thank you