This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC1825: Opel loop operation of UC1825

Part Number: UC1825

Hi, I am currently using the UC1825 in open loop mode. And I see the following waveform in at the output of the error amplifier (where the output is expected to be DC). Is there a possible explanation for this operation

Thanks

  • Hello Nandha

    Please check the INV and NI inputs to the error amplifier. If I wanted to run this device open loop I would ground the INV input and tie the NI input to VREF. If this doesn't solve your issue then please post your schematic here -

    I hope this helps

    Regards

    Colin

  • Hi Colin,

    Grounding the INV input to ground would drive the IC to its full duty cycle limit (the voltages are fine in this config). I want to control the duty cycle of the output using a 10k pot. Doing so led to this result. Any other way to control the duty cycle in open loop

    Thanks and regards

    Nandha

  • Hello Nandha

    You can configure the on-board error amplifier as a voltage follower by connecting INV to E/A OUT and putting a DC voltage on the NI pin. The DC voltage will control the duty cycle linearly once NI is between about 1.25V and 4V.

    A 10k pot from VREF to GND should work nicely.

    Regards