This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54528: lower current limit setting

Part Number: TPS54528

Hi Team,

The TPS54528 is a 5A output IC. Is there any way to set the overcurrent protection to 5A or less?
Currently, the overcurrent protection function operates at an output current of 5.5A, but I want to operate it at about 3-3.6A.

For example. If the inductance of L1 is reduced, the current swing inside the IC will increase, and as a result, is there any way to set the OCP?
It is assumed that it is necessary to respond to changes in electrical characteristics during steady operation as much as L1 is lowered.
Any advice should be highly appreciated.
Thanks
Best regards,
Shidara