Other Parts Discussed in Thread: TLV755P, , LP5912, TPS745
Hi All,
I would like to know the difference between CMOS LDO(LP38693) and PMOS LDO(TLV755P).
Do we have the technical document between them?
Roy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Roy,
Both devices are CMOS based devices.
They both use PMOS pass elements.
We could help review the different specifications between the two devices using our online LDO tool, which you can see here, to help you down select between the two, if that helps.
I'll add someone from our marketing team to aid in selection of a P2P device with the AP7217 component.
Thanks,
- Stephen
Hi Roy,
Unfortunately I could not find an exact drop in from our portfolio. However we have many LDOs that have a similar function. We typically call this VDOUT a power good or reset pin.
In TI we have many devices that can perform similar to AP7217. Our TPS745 is our latest released family of 500mA LDOs with integrated power good (reset) but features a wider voltage operation. You can also look at our LP5912 family for fixed output voltage regulation with a power good pin.
Dear Stephen,
Thank you for your reply. I have this question because I review some LDO datasheet, some is showing they are CMOS LDO, the other are not showing. Like I mentioned previous. Why they show they are CMOS LDO, is that a special point that we could promote?
Regards,
Roy
Hi Jose,
Thank you for your reply, I will choose the suitable part to customer.
Regards,
Roy
Hi Roy,
There are pro's and con's to CMOS and other types of transistor based LDO's.
The main technology which competes with CMOS is called bipolar junction transistor (BJT).
Most integrated circuit design is now CMOS based, so it would be hard to point at that and use it to promote a component, as the competitor's component is likely also CMOS based.
A good resource which gives the basics of BJT based linear regulators can be found here.
http://www.ti.com/lit/an/snva558/snva558.pdf
Another good resource which discusses both BJT and CMOS based linear regulators can be found here.
http://www.ti.com/lit/an/slva072/slva072.pdf
Thanks,
- Stephen