Hello,
I am currently working with the tps7a4701. Here is the schematic.
The 28V bus is attached to a battery, which can vary from 26V to 32V. The issue we are seeing is that every once in a while the part will die. We will replace it and then about a week or so later we see it die again. Any ideas as to what might be going on?
The current being pulled is less than 0.5A.