This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3422: Option to connect the TS pin to VCC for tTIMER delay of 0s

Part Number: TPS3422

The data sheet of TPS3422 shows the option to connect TS pin to either VCC (for tTIMER = 0s) or GND (for tTIMER = 7.5s). 

But in the 'Timing Requirements' section (section number = 6.6) it is given as a note that TS = VCC is only for factory testing and is not intended for normal operation. In normal operation, the TS pin should be tied to GND.

Can I have a clarification about this. Can I connect the TS pin to VCC for '0s' delay ?