Other Parts Discussed in Thread: TIDA-00711, PMP21488
Hi, TIDA-00711 based on LM5020 is an ISOLATED 50W DC to DC converter. However, in schematic on page 6 of the design document, the DC input ground is labelled as PGND and the main secondary 12V , 3A return is also mentioned as PGND !!!!
If input ground and the secondary ground are the same then is it isolated DC to DC converter ?
Regards
Atul BhakayLM5020_design_tiduco3a.pdf