Team,
Customer need a precise Vout (fluctuation < 0.1% Vout) at low load for his application:
Vin: 5V, Vout: 3.3V, Iout typ: between 70mA to 85mA, Iout max: 200mA
-Do we have some more precise measurements for the PFM to PWM transition?
Fig.4 page 7 of SNVS250F datasheet does not easily enable to assess the values for 3.3V.
Do we have the theoretical PFM/PWM transition levels for 3.3V Vout?
-On the current HW we measured 80mA for PWM-> PFM and 110mA for PFM -> PWM.
Do we have information of those transition vs temperature?
-Do we have some simulation models that would help simulate this behavior?
Thanks in advance,
A.