Other Parts Discussed in Thread: TLC59108F, , TLC59108
Hello Community,
i would like to be sure of the differences between TLC59108F and TLC59208F.
This E3E topic describes
that the difference between TLC59108 and TLC59108F are just the output structure. (Current-Source / Open-Drain)
that is Open-Drain for both.
HW wise i found
parameter | TLC59108F | TLC59208F |
---|---|---|
Maximum Output Current | 120mA | 50mA |
the Functional Block Diagram
is also about the same for both:
the only other difference found is with Regular I2C Bus Slave Address
:
there fore the TLC59208F has much more possible addresses.
are there any other differences i missed?
and are the three parts (TLC59108, TLC59108F, TLC59208F) interchangeable from a I2C view?
(so i can switch the parts later if needed but don't need to change software?)
thanks for any feedback!
sunny greetings
stefan