Hello,
I am looking for a single LDO to convert
Input Voltage: 3.5 V
Output Voltage: 1.1 V
Current: 0.5 A
Hence Vin > Vout +1.62, I do not need a Vbias. I can connect Vbias and Vin to the 3.5 V rail with a single 4.7 uF capacitor. Is this correct?
Thanks,
Vibhu