Other Parts Discussed in Thread: TPS3600, TPS3610
Dear,
I am using TPS3606 and i have observed that when the WDI pin is pulled high to 3.3V , at this point the WDI had voltage pulsating from 3.3V to 3.15 (ON-OFF-ON state) and the /RST pin is generated pulses with 110mS on and 900mS off. Why is this erroneous behavior ?
Can also suggest similar IC , where both VDD and VBAT can be used for powering the uC and whenever VBAT goes less than xx threshold the device disable the output and no power is available to controller.